Categories
Knowledge Support Support exacqVision Server Categories Products

Illustra3 links device level connection to video stream

Description

Illustra3 supports a separate http socket to stream metadata such as analytic/motion/input trigger. This allows the device level support of events independent of the video stream. Which provides a device level connection state that could be use to monitor the device.

<br>

Version Introduced

r52213 (RC 5.10.x)

<br>

Platform

All

<br>

Steps to reproduce

illustra3 camera(625/825/mini-dome/mini-bullet/Pro/Flex)

program an “IP Camera Connection” event linking for the illustra3 device connection.

disable streaming recording.

<br>

Expected result

stream connection disabled.

device connection is connected and input trigger still available.

<br>

Actual result

stream connection disabled.

device connection is also disconnected with the video stream.

<br>

Work Around

none

<br>

Version Fixed

none

<br>

Keywords

Illustra3