The installer for the following specific version has an option to install postgresql even if it detects a postgresql installation on the machine, however it does not work. It throws an error as it is not able to set the install path correctly.
Tested Version
3.6.0
Platform
Windows
Steps to reproduce
- Install postgresql by hand
- Run ESM installer, select install postgresql on dialogue popup
Expected result
Installation completes of postgresql
Actual result
Error in trying to install
Introduced Version
r82419
Work Around
Do not attempt to install postgresql if it is already installed.