Changing/Testing advanced ESM settings manually

For some more advanced settings/options on ESM, navigate to ESM installer directory/folder. Here on the commandline as an admin user, you can use the installer.exe (windows), or installer executable for different actions.

<br>

Check/Change database settings

Commands to run:

Linux:

  • sudo ./installer decrypt (will generate EnterpriseManager.tmp – View or change settings here)
  • sudo ./installer encrypt (do this only if you changed settings)

<br>

Windows:

  • installer.exe decrypt (will generate EnterpriseManager.tmp – View or change settings here)
  • installer.exe encrypt (do this only if you changed settings)

<br>

Encrypt Results:

  • -3: EnterpriseManager.tmp does not exist in the current directory
  • -2: The tmp file could not be opened
  • -1: EnterpriseManager.ini could not be opened
  • 0: EnterpriseManager.ini has been created in the current directory

<br>

Delete the EngerpriseManager.tmp file.

Note: If you have changed database settings. Restart all esm services. Preferably, starting with the importer Verify ESM is functioning as expected.

<br>

Test Migrations 

(checks conditions for running a migration and returns an integer value)

Commands to run:

  • sudo ./instaler testmigration (Linux)
  • instaler testmigration (Windows)

<br>

Results:

  • -3: no default database connectivity
  • -2: nolegacy database connectivity
  • -1: migration has already ran
  • -0: it is okay to run a migration if wanted

<br>

Run database migrations 

(runs the actual migration and returns an integer value)

Commands to run:

  • sudo ./installer runmigration (Linux)
  • sudo ./installer runmigration (Windows)

<br>

Results:

  • -1: migration succeeded

<br>

Run ESM diagnostics

Currently this will run diagnostics for Email and Domain server connectivity

Commands to run:

  • sudo installer diagnostic (Linux)
  • installer.exe diagnostic (Windows)

<br>

Update the haystack search indexes 

(adds missing entries)

Commands to run:

  • sudo ./installer update_index (Linux)
  • sudo ./installer update_index (Linux)

<br>

Test connectivity to the given database

Commands to run:

  • sudo ./installer testconnection (Linux)
  • installer.exe testconnection (Windows)

<br>

Test the given port for availability

Commands to run:

  • sudo ./installer testport [port] (Linux)
  • installer.exe testport [port] (Windows)

<br>

Results:

  • -1: no connectivity
  • 0: in use

<br>

Test the given SSL port for availability

Commands to run:

  • sudo ./installer testsslport [port] (Linux)
  • installer.exe testsslport [port] (Windows)

<br>

Results:

  • -1: no connectivity
  • 0: in use

<br>

Get an available port starting at startport

Commands to run:

  • sudo ./installer getfreeport [startport] (Linux)
  • installer getfreeport [startport] (Windows)

<br>

Get an available SSL port starting at startport

Commands to run:

  • sudo ./installer getfreesslport [startport] (Linux)
  • installer getfreesslport [startport] (Windows)