Honeywell Vista 128bpt Incorrect Bypass Status

Issue

An issue was found with our Honeywell Vista Security Integrations plugin and the Honeywell Vista 128bpt panel where the zone bypass button was not functioning for some combinations of zone status.

Each zone is capable of having up to 16 different states simultaneously. For example, a zone may be in a state of both ‘alarm’ and ‘open’.

Certain combinations of states would cause the panel to send us a message which the plugin was parsing improperly.   This would cause the Client to display an incorrect zone bypass status (for example, the zone might actually be bypassed, but the client would show un-bypassed).

<br>

Version Affected

19.12 or lower

<br>

Version Fixed

20.03