Axis crash server with date/time settings

Description

Server crashes when add Axis camera with date/time on the camera is set to sync manually or with computer time.

<br>

Version introduced

8.6.1.115070

<br>

Platforms

All

<br>

Steps to reproduce

  1. In the camera web page, change the “Time mode” to either manual or with computer time in “Date & Time Settings” page.
  2. connect Axis camera to 8.6.x server.

<br>

Expected result

NTP is sync either to server or override setting.

<br>

Actual result

Server crashes.

<br>

Workaround

Manually set “Time mode” to “Synchronize with NTP server” option.

<br>

Version fixed

8.7.8.115465

<br>