Issue
Cameras will not record on motion due to a firmware issue. Currently there is a ticket that needs to be re opened and worked on with Illustra.
Motion will not work on JPEG/H264/H265 if the camera was originally configured with the Enhanced Security Mode enabled by default.
<br>
Workaround
Default the camera and log into the GUI of the camera and select Standard security mode.

<br>
Version Affected
All