Categories
Knowledge Support Support exacqVision Server Categories Products

Crash when deleting UDP serial port

Description

Server crashes when deleting a UDP serial port. The crash happens for both the stand-alone UDP serial port or the Neo internal serial port.

<br>

Introduced

8.4

<br>

Workaround

Workaround is to disable the UDP serial port before deleting it. To disable a stand-alone UDP serial port, set the usage type to None. To disable the integration serial port, disable the integration connection.

<br>

Fixed

8.5.x.