Feature – Axis Body Worn Cameras
- Client – Enhancement – Axis body worn camera support. #21843
- Client – Enhancement – Added support for search only cameras and audio for Axis body worn.
- Client – Enhancement – Added config options for axis body worn cameras.
- Server – axisbwpi – Add support for the Axis body worn camera system #21204
Feature – Large Blobs
- Client – Enhancement – Support Large Blobs. #21842
- Server – Enhancement – streampi – Support for maps and other blobs of sizes exceeding 2MB #18412
Client
- Enhancement – Automatically create a system event linkage for source groups in event monitoring. #22396
- User will be warned if trying to delete an automatically created Event Link
- Enhancement – Allow selecting multiple files at once in Add Person #21332
- Enhancement – Updated Immervision libraries for newer camera model support. #22384
- Enhancement – Upgraded Oncam dewarping library for newer camera support. #21914
- Enhancement – Added Linux x64 support for Oncam dewarping. #21914
- Windows and Linux only
- Mac library not ready
- Enhancement – Enterprise LDAP: enable local user accounts checkbox if connected as a local user AND local user accounts are disabled #21933
- Enhancement – For enterprise and system LDAP pages, disable the option to disable local user accounts if current use is local #21933
- Enhancement – Added timeout message to export log if we timed out waiting for system or audit logs during support export. #22417
- If cancelled, then the next export wouldn’t include the Server logs.
Server
- Feature – rtspserverpi – Add support for video search #20747
- Backend search capabilities without needing to use our API.
- Primarily for future projects.
- Enhancement – AxisPI – Support events for Axis Fence Guard #22465
- Similar to Line Cross.
- Must be configured in the camera with a browser.
- Enhancement – AxisPI – Improve performance of downloads from edge storage #22303
- 5m sub-operations to split up data and better protect against lost video due to network disconnection.
- Parallel downloads – Off by default, must be configured.
- Enhancement – AxisPI – change to more efficient log format #22502 §Similar to Onvif/Illustra
- Enhancement – Illustra3pi – Correctly identify Holis cameras #22222
- Some were improperly added from the scan as Onvif before.
- Still using the Illustra3 plugin but will show up in the Client as Hollis.
- Enhancement – onvifnvcpi – Add Support for Vivotek MA9321/2-EHTV #22373
- Other json updates for specific cameras as well.
- Enhancement – onvifnvcpi – Add the Subscription Renew command to pullpoint if MaxNotificationProducers capability is detected. #22165
- Resolves some of the “Motion not supported” messages.
- Enhancement – onvifnvcpi – Add override for cameras that prefer GetCapabilities instead of GetServices. #20941
- Enhancement – plugins – hardened config persistence against unexpected shutdowns #15944
- Changes in how config file gets edited and saved.
- *.xml.bak created first
- Changes saved to *.xml.pending
- *.xml.pending then renamed to *.xml
- Changes in how config files are loaded.
- *.xml.pending is always most recent save. Load it first
- Then try *.xml
- Then try *.xml.bak
- log load/save errors for core.xml.
- Changes in how config file gets edited and saved.
Web Service
- Enhancement – Add ability to monitor and remove temporary files. #22276
- Thumbnails and Search results
- Now cleaning up after 12 hours.
- Enhancement – Add RTSP URI to camera endpoint. #22568
- API feature – no UI
- Will be utilized by Integrations
- Enhancement – Sort available update versions, newest first. #18059