SCN-00000011 – G-Series Micro

SCN #SCN-00000011
Title of SCNG-Series Micro
TRAC #
Effective VersionLaunch tentatively scheduled for March 22, 2019
Products AffectedN/A
Reason for Change (Summary)New Product

Change

The G-Series Micro is designed to provide a low-cost “gateway” option to the new Cloud Drive service.  The machine will come with 2 Professional licenses.

Specs:

  • Intel Celeron (J3455)
  • 2GB DDR RAM
  • Dual Gb NICs
  • HDMI and mini DP monitor outs
  • 1 TB 2.5inch HDD
  • 4 USB Ports
  • Palm size form factor
  • Ubuntu 16.04
    • Includes the standard exacqVision Linux image comparable to Z, S, A and LC Series machines.

Key Differentiators

  • Low storage capacity
  • Small Form Factor
  • Fan-less, quiet

Additional Documentation

Quick Start Guide coming soon…

Other information

This machine should be troubleshot similar to any machine with the standard exacqVision Linux image.  Like the LC, the Operating System will reside on the spinning Hard Drive.  If the drive is replaced, the machine will need to be re-imaged.