Unable to Connect to Panasonic Device with FW 1.03 or 1.10

Symptom:

Connection to Panasonic device is stuck in “Connecting” despite displaying the model and MAC address.

<br>

Problem:

The following Panasonic devices were found to return an invalid image size when using firmware 1.03 or 1.10. 

  • WV-S1550L
  • WV-S2131L
  • WV-S2250L
  • WV-S2550L
  • WV-S8530N
  • WV-X8570N

<br>

Solution:

Panasonic is planning to release a firmware update to address this issue.

<br> 

Unable-to-Connect-to-Panasonic-Device-with-FW-1.03-or-1.10-2.pdf