Dewarper Workaround

Issue

Both Axis and Pelco depend on OpenGL for dewarping.  If dewarping is not working for a Windows client because of GPU driver issues you can use the following open source Mesa3D software OpenGL drivers as a work around.  This will basically use a software implementation of OpenGL to do the dewarping which is really no worse than 90% of the other dewarping libraries anyway. It will not perform as well as if it were using the GPU OpenGL drivers, but it seems reasonable.  CPU usage went from 6% using GPU drivers to 12% using these drivers.

<br>

Workaround

  • Download Mesa3D windows binaries from https://github.com/pal1000/mesa-dist-win/releases
  • Extract contents of either x64 or x86 folder to client install directory depending on which client is installed
  • OpenGL32.dll should be in the same folder as edvrclient.exe

<br>

Dewarper-Workaround.pdf