In version 4.1 of the ExacqVision software, advanced RS-422 PTZ controls were implemented for Pelco-D and American Dynamics domes. One of the advanced controls allows the operator to open the dome’s internal menu to display menu choices in an onscreen display (OSD) embedded in the dome’s video stream. A cursor can be moved up and down the menu using the ExacqVision Client’s PTZ up and down arrow controls.
<br>
Pelco-D
- To select item at cursor: Iris Open
- To change selected value: up and down arrows
- To exit menu: move the cursor to the Exit menu item and select
<br>
American Dynamics
- To select item at cursor: Focus Far
- To increase the selected value: Zoom In
- To decrease the selected value: Zoom Out
- To exit menu: either move the cursor to the Exit menu item and select, or use the exacqVision Client’s Menu Off command
<br>