Intel Desktop Utilities for Windows 7

NOTE: It is recommended that you do NOT install this software on Windows XP Professional.

<br>

You can download Intel Desktop Utilities from the following location:

http://downloadcenter.intel.com/Detail_Desc.aspx?agr=Y&DwnldID=18934&ProdId=3121〈=eng

<br>

If you are not using the server and need to manually download the drivers, complete the following steps:

<br>

  1. Select Desktop Boards under Products.
  2. Select Intel® 4 Series Chipset Boards under Product Line.
  3. Select Intel® Desktop Board DB43LD under Product Name.
  4. Select Windows 7, 32-bit under Operating System.
  5. Select Software Applications under Download Type.
  6. From the list, select Intel® Desktop Utilities from 4 & 5 Series Desktop Boards.
  7. Follow the links and download the software.

<br>

If you are on the server itself, you can have Intel automatically search for the drivers and software needed. To do this, complete the following steps:

<br>

  1. Click Run Now under the Automatically Identify and Find Drivers section.
  2. After the IDU_x.zip file is downloaded (x is the version of IDU software), extract the files to the Desktop (by default, they extract to an IDU_x directory).
  3. Open the directory where the ZIP file was extracted to. Right-click Setup.exe and select Run as Administrator to install the program.

<br>

To make exceptions in Windows Firewall, complete the following steps:

<br>

  1. Click Start, Control Panel, and Windows Firewall.
  2. Select Allow a Program or Feature Through Windows Firewall.
  3. Click Change Settings.
  4. Confirm the action if the UAC appears.
  5. Click Add Another Program.
  6. Click Browse.
  7. Browse to C:\Program Files\Intel\Intel Desktop Utilities.
  8. Select intelmain.exe and click Open.
  9. Repeat steps 5-7 and select iptray.exe and click Open.
  10. Confirm that Intel(R) Desktop Utilities and Tray Application for Intel(R) Desktop Utilities have been added to the exceptions list.

<br>

You have now installed Intel Desktop Utilities to your Windows 7 exacqVision Server.

<br>

Intel-Desktop-Utilities-for-Windows-7.pdf