Categories
Knowledge Support Support exacqVision Server Categories Products

Creating a Shutdown Hot Key in Linux

To create a shutdown hot key on a Linux ExacqVision system, complete the following steps:

Ubuntu 20.04 & 18.04

These systems are already configured to use CTRL+ALT+DEL to pop up a dialogue with a shutdown option. Once the dialogue opens the system will shutdown if no further user interaction occurs.

Ubuntu 16.04 and earlier

This requires advanced customization using donf-editor which is beyond the support provided by Exacq Support. Users perform any such customization on their own.

<br>