Can the Web Server run on an Exacq EL NVR system?

Yes, exacqVision EL supports a Web Server used to provide the mobile device video access. The Web Server is not installed on EL by default because if it runs simultaneously with exacqVision Client on the EL hardware, performance of both the local client and the Web Server could be noticeably slower (this is the tradeoff for the low power consumption and reduced cost of the Intel Atom processor). The loading introduced by the Web Server is roughly equal to the client. Remote clients connected to the exacqVision Server do not introduce significant CPU loading.

<br>

On exacqVision ELP systems, the Intel Celeron processor can run exacqVision Client and Web Server simultaneously. exacqVision Client performance is still dependent on the processor. See Client Workstation Hardware Requirements on this page for more information.

<br>

The installation of the Web Service is very easy and no different than for any other Ubuntu Linux-based system. The Web Service installer is available at https://exacq.com/support/downloads.php.

<br>