To troubleshoot an eDVR board, complete the following steps:
- Download Microsoft’s DebugView program from http://technet.microsoft.com/en-us/sysinternals/bb896647.aspx<br><br>
- Open the file
C:\Windows\xdvapi.ini
Note: In Windows 7 or Windows Vista, run Notepad as an Administrator and then select Open from the File menu and change the file type to ‘All Files (*.*)’ to open the INI file.<br><br> - Find the
[CONFIG]
section, or create it if necessary.<br><br> - Add a line after
[CONFIG]
as follows:[CONFIG]
ODSFlags=0x80000003
<br><br> - Run the DebugView application.<br><br>
- Stop the ExacqVision Server service.<br><br>
- Start ExacqDV Control Center. Several lines of information will scroll in the DebugView window. Click Clear in the DebugView toolbar.
Note: The Clear button looks like an eraser and a piece of paper and can be found below the Help menu.<br><br> - In the ExacqDV Control Center tree, select the eDVR board that you want to troubleshoot. A “-9005” error will appear along with additional information in DebugView.<br><br>
- Copy the information from DebugView into an email and send it to support@exacq.com.
<br>