Get the Monitor Size (resolution) Back for Linux Sy stems

The monitor can get stuck in 640*480 mode if the system is booted with no monitor connected.

To get the monitor size back for Linux systems, complete the following steps after opening Terminal:

  1. Type cd /etc/X11
  2. Type sudo mv xorg.conf xorg.bak.conf
  3. Restart the system with a monitor attached.

<br>

Get-the-Monitor-Size-resolution-Back-for-Linux-Systems.pdf