Using Panasonic Input Triggers

When a digital input is triggered on a Panasonic camera, the camera transmits a single alarm to indicate the condition. This means that the triggered state cannot be seen on exacqVision Client’s Trigger Input page. To test Panasonic digital inputs, you must use them with Event Linking or Event Monitoring.

< br>

Using-Panasonic-Input-Triggers.pdf