Categories
Knowledge Support Support exacqVision Server Categories Products

Configuring SSL on an exacqVision Server for Active Directory/LDAP (Linux)

exacqVision 7.2 and higher:

Check the box labeled “Use SSL” on the “ActiveDirectory/LDAP” configuration page, then press “Apply”.

<br>

exacqVision prior to 7.2:

This article contains procedures for configuring SSL on exacqVision servers so that you can make Active Directory operations more secure.

There are many ways to generate, install, and manage certificates in order to use SSL, but this document explains one simple option: exporting the trusted root certificate that already exists in your Active Directory domain and installing it on each exacqVision server.
<br>

Export Trusted Root Certificate for Your Domain

  1. Log in to any Windows workstation that has already been added to your domain. The login account must have at least local admin permissions.
  2. Start the Microsoft Management Console (mmc.exe).
  3. If you haven’t already, add the Certificates snap-in:

    a) On the File menu, click Add/Remove Snap-In.
    b) Select Certificates and click Add.
    c) When prompted, select the option to manage certificates for your user account (instead of the service or computer account).
    d) Click Finish.
    e) Click OK to complete this step.
  4. Expand Certificates – Current User in the left pane.
  5. Expand Trusted Root Certification Authorities.
  6. Select the Certficates folder to display your workstation’s currently installed CA certificates. The Issued To field should contain something similar to mydomain-ROOT-CA, where mydomain is your domain name.
  7. Select that Issued To entry, right-click All Tasks, and select Export.
  8. In the Certificate Export Wizard, select the format choice of Base-64 encoded binary X.509 (.CER). Save it to a local .cer file that you can relocate later. You will then install this same certificate file on every exacqVision Server for which you intend to use SSL.

<br>

Certificate Database Location on exacqVision Server

Whenever exacqVision Server attempts to connect to an Active Directory server, it creates the following files in the installation directory, if necessary:

cert8.db
key3.db
secmod.db
<br>

Import Trusted Root Certificate into Each exacqVision Server

  1. On the exacqVision server, copy your trusted root certificate to the server’s installation directory at /usr/local/exacq/server.
  2. If you have not already verified your exacqVision Server’s LDAP configuration with SSL disabled, do this now. This will create your certificate database files if they do not exist already.
  3. Open a Terminal window and type the following:

    sudo openssl s_client -connect FQDN:636 -ssl3 | sed -ne “/-BEGIN CERTIFICATE-/,/-END CERTIFICATE-/p” > ad.pem && sudo mv ad.pem /usr/local/exacq/server
    where FQDN is the fully qualified domain name of your Domain Controller.
  4. Press Enter twice to create the .pem file and move it to the Servers directory.
  5. Change to the exacqVision server’s directory with

    cd /usr/local/exacq/server
  6. Run the following two commands:

    sudo certutil -d . -A -t “C,C,C” -i MY_CERT_FILE -n adca

    where MY_CERT_FILE represents your trusted root certificate file; and

    sudo certutil -d . -A -t “u,u,u” -i ad.pem -n ad
  7. In a Terminal window, restart your exacqVision server with the following command:

    sudo service edvrserver restart
  8. On your exacqVision server, run exacqVision Client and open the Active Directory/LDAP tab. Select the SSL checkbox (the port should automatically change to 636), and then click Apply. Your exacqVision Server should then reconnect to your Active Directory domain controller.

<br>

Configuring-SSL-on-an-exacqVision-Server-for-Active-Directory-LDAP-Linux.pdf