Pelco SMLE1-15V5-3h Motion Events are not Received by Exacq

Description 

The Pelco SMLE1-15V5-3h does will not record or see last motion events in exacq client/ server.
Both Firmware’s were tested and work with the override.
4.80.0.24(F722c136)
and
fw 4.86.0.20(7a7d6563)

Product 

ExacqVision Server 24.03.7.0 – 24.09.4.0

Steps to Reproduce 

Set up motion in the cameras gui for each head in the camera to enable motion events.

Expected Results 

Exacq should receive Motion Status events and record.

Actual Results 

Motion Events are not seen by exacq while camera is sending motion events, and Exacq does not record. Continuous Recording Does work.

Solution

Update: 24.12.7.0 has been successfully tested and working with the overrides.
#Config=dynamic
AES-1069
This will be addressed in a future official release to remove the need for the overrides when adding these cameras.
Until them please update to server to the 24.12.7.0 version and use the overrides as needed.

<br>