Installing A-Series Rails on Racks with Threaded Round Holes

The rack mount rails that ship with exacqVision A-Series NVRs are designed to be toolless when used with server racks that have square or unthreaded round mounting holes on the rack uprights. The following guide describes how to adapt these rails, using tools, for use with rack uprights with threaded round screw holes.

  1. Examine the each end of the rail and take note of the pegs, as indicated in the illustration below.
  1. Insert a Phillips-head screwdriver into the slot at the end of each peg and turn to remove the pegs. Repeat this on the opposite end of the rail. The rear end does not have a center peg.
  1. Each end of the rail should have all pegs removed.
  1. Depending on the spacing of the holes on your rack, the L-bracket on the end of the rail may fit around the upright, facing outward, or may need to be placed behind it, as pictured. Here, the screw threads through the rack and then into the threads on the end of the rail where the pegs you removed from previous steps were located. Use installer provided screws to secure the rail to the rack’s upright.

<br>