Replacing a Hard Drive on Q-Series 2024 Refresh

  1. Looking at the rear of the system, remove the three screws indicated in the illustration below.
  1. Looking at the rear end of the top cover, remove the two screws indicated below.
  1. Slide the top cover towards the rear and pull off to remove it from the chassis.
  2. Remove the three screws indicated below.
  1. Remove the front bezel by lightly lifting the tabs indicated and rotating the top of the bezel away from the chassis.
  1. With the front bezel removed, looking at the front of the system, remove the two screws in the upper corners as indicated in the image below.
  1. Lift the drive plate to separate it from the chassis. Remove the hard drive retaining screws shown in the image below, supporting the drive from underneath.
  1. Detach the SATA power and data cables from the hard drive and attach to the replacement drive. Reverse the steps above to reassemble the system.
  1. When reattaching the drive plate, fit the three tabs on the front of the plate into the slots as shown.

<br>