Exempt Files Targeted by Antivirus Scans

*** INTERNAL USE ***

Antivirus Configuration

As with all third-party software not on the Product Integration section, the user assumes the risk of software incompatibility with the exacqVision software suite.

Therefore, if there is an inquiry on what an AV program found and is blocking we should open a ticket with engineering and confirm what the file is, and what it does to help maintain a list of examples that can be excluded.

It is recommended to exempt certain files if they are targeted by scans of the Antivirus program to allow proper functionality of the software.

List of examples for certain scans and why they are important for Exacq Software. The file extension may be ‘.exe’, ‘.ps’ or ‘.ps.1’ for Windows. In Linux it will be ‘.sh’.

  • curl – Utilized to download updates, email and sync with EM.
  • dhcpconfig – Utilized for enabling/configuring the DHCP Server
  • driveprep – For partitioning new data drives.
  • dvdrwtools – For burning of a DVD/CD.
  • dvd+rw-mediainfo – For burning of DVD/CD.
  • evselftest – Utilized to scan disks for errors.
  • failover – Utilized for failover/failback.
  • iscsiprep – For configuring Extended volumes.
  • lshw – Utilized to gather hardware/software information about a system.
  • mediainfo – For burning of DVD/CD
  • mdnsd – For discovery of IP devices, Servers and Clients.
  • mDNSResponder – For discovery of IP devices, Servers and Clients.
  • mkbadst_config – For configuring Extended volumes.
  • mount – For mounting new data drives.
  • netconfig – For configuration of Network Interface parameters.
  • ntpd – For management of Time Servers and synchronization.
  • ntpdate – For management of Time Servers and synchronization.
  • opendhcpd – Utilized for enabling/configuring the DHCP Server
  • opendhcpserver – Utilized for enabling/configuring the DHCP Server
  • parted – For partitioning new data drives.
  • rmfs – For partitioning new data drives.
  • smartctl – Utilized to gather health (S.M.A.R.T.) data from drives.
  • sysinfo – Utilized to gather hardware/software information about a system.
  • teaming – For creating NIC bonds.
  • tzutil – For configuring the Time Zone settings of the OS.
  • update – Utilized to download and install updates as well as failback of recorded data.
  • w32time – – For configuring the Time settings of the OS.
  • wodim – For burning of a DVD/CD.
  • winio – This script is part of sysmgmtpi which monitors the health of the server and drives. The winio64.sys is the driver that allows part of that functionality.

<br>

Related Articles

Using Antivirus Software with exacqVision

<br>