Categories
Knowledge Support Support exacqVision Server Categories Products exacqVision Hardware

How to Determine the Age of a System Using a Serial Number

Exacq hardware serial numbers include both the year and the week number the system was built. See How to Find the Serial Number of an exacqVision System for help in finding your system’s serial number.

There are a few different serial number prefixes depending on where the system was built. They are:

  • D14A
  • AV
  • ER
  • 355S
  • BH
  • SR

After this, the next 2 digits will indicate the year – for example:
D14A2408123456
This system was built in the year 2024.

Next you will find 2 digits that indicate the week number – for example:
ER2408123456
This indicates that the system was built in the 8th week of 2024.

The remaining numbers are incrementing unique identification numbers.

<br>