Categories
Knowledge Support Documentation Support exacqVision Server Categories exacqVision Hardware Products

RS-485-to-USB Adapter Compatibility with ExacqVision

Two RS-485-to-USB adapters have been tested for compatibility with exacqVision: B&B Electronics, model 485USB9F-4W and VSCom, model USB-COMi-TB. The tests used the drivers supplied with the devices, and data has successfully been transmitted and received to and from each adapter. They were also tested in a loopback configuration with the RS-485 port built into an exacqVision server equipped with an analog capture board.


B&B Electronics, model 485USB9F-4W

VSCom, model USB-COMi-TB


Installation

  1. Install the adapter driver (included with the device or downloaded).
  2. Plug the device in to the USB port of the exacqVision server.
  3. Ensure that Windows discovers and configures the device properly. (Use Device Manager, found in Control Panel.)
  4. Restart the exacqVision Server service.
  5. In exacqVision Client, open the Serial Ports page.
  6. Verify that a new COM port exists in the UART section of the Serial Ports page.
  7. Configure the port as you normally would for PTZ control output or POS data input.

Notes

  1. The B&B adapter is equipped with a standard D-sub, 9-pin, female connector on the RS-485 side. A pinout diagram is included with this device.
  2. The VSCom adapter has terminal blocks on the RS-485 side, allowing easy connection of bare wires. The dip switches and jumpers were left in their default settings for testing.

<br>