AVI/Quicktime Codecs

The following table contains information about the recommended codecs when exporting video from the exacqVision Client or ePlayer to *.avi format for playback in Windows Media Player or *.mov format for playback in Quicktime on Windows or Mac platforms. In Windows and Linux, video exported in either *.avi or *.mov format can also be played back using VLC without requiring any codecs that are not installed by default with VLC.


Quicktime and AVI File Export Players


You can download players at the following URLs:

Windows Media Player
http://www.microsoft.com/windows/windowsmedia/default.mspx

Quicktime Player
http://www.apple.com/quicktime/download/

VLC Player
http://www.videolan.org/vlc

MPlayer
http://www.mplayerhq.hu/design7/dload.html


You can download codecs at the following URLs:

3ivx MPEG4 decoder
http://store.3ivx.com/3ivxStore/?features=dec&platform=win&license=plus&Go=Go

DivX decoder
http://www.divx.com/en/downloads

Quicktime codec resources
http://www.apple.com/quicktime/resources/components.html?os=Windows&ctype=696d6463&csubtype=48323634

Perian Codec for Quicktime
http://www.perian.org

AVI-Quicktime-Codecs.pdf