Video may be exported from exacqVision in different formats. The table below illustrates some of the differences in these formats.
Multi-Camera: For the purposes of this article, multi-camera means many camera streams are combined into a single exported file. When exporting as .MOV, .AVI, or .MP4 each stream will end up as its own file.
Self-Playing: The .EXE file format bundles the exacqVision ePlayer into the file. This allows the file to be opened and played back on any Windows desktop or server operating system. This file format does not play natively on Ubuntu/Linux or Mac systems.
For more details on .AVI and .MOV usage and codecs, please refer to Article 1925
<br>