ASRock Industrial IMB-X1313 System Beep Codes

Beep SequenceDescriptionTroubleshooting
1 short constant beepError with RAM refresh1. Check RAM for physical damage.
2. Try another stick of RAM.
3. BIOS update
2 short beepsRAM parity error1. If adding new memory, try removing to see if this fixes issue.
2. Check for conflicts in memory types.
3. Check power supply for unstable voltages.
3 short beepsRAM read/write test failed1. Repair corrupted files.
2. Perform memory tests
4 short beepsSystem clock errorTry synchronizing system time with an internet (NTP) time source.
5 short beepsCPU errorCheck that CPU is properly seated.
6 short beepsKeyboard not detected/
keyboard controller error
Check keyboard is properly connected or try a different keyboard.
7 short beepsGeneral CPU or RAM error1. Check that CPU is properly seated and connected.
2. Check that RAM is properly seated and connected.
3.Inspect connections for dirt or corrosion.
8 short beepsGraphics controller errorCheck for proper connections to any graphics cards installed and that enough power is provided to the card.
9 short beepsROM errorCheck if system is attempting to boot from an external device.
10 short beepsROM read/write error1. Run a memory diagnostic, such as mdsched.exe in Windows.
2. Clear CMOS
11 short beepsCPU cache check failure1. Check CPU temperature.
2. Inspect CPU fan for proper function.
3. Clear dust or dirt from CPU fan.
4. Check for faulty CPU heatsink.

<br>