Categories
Knowledge Support Cloudvue Cloudvue Cameras Cloudvue Gateway Support Categories Products

Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif

Description

Prior to the release of Cloudvue version 23.9 the error message “”Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif'” could appear when trying to add cameras to a Cloudvue Gateway.

This will be fixed with the release of 23.9.

Products 

  • Cloudvue Gateway v 22.9.x and older
  • Hikvision
  • Illustra
  • ONVIF

Steps to Reproduce 

Add a new camera either by scanning or by IP.

Expected Results 

Camera adds to the system.

Actual Results 

Camera does not add and displays the error “Error: Cannot find module ‘@jci-Internal/acvs-cloudvue-onvif”.

Solution

  • Use Cloudvue Manager to Update the Device
  • If the version is 23.9.x or higher then try to add the camera again
  • Otherwise, contact Cloudvue Support, they will help you in getting a support case started which will be escalated to L3 support who can remotely resolve the issue.