Description
Adding an Amcrest camera as ONVIF to a Cloudvue Gateway fails with an error message “Invalid Username / Password”. This is true even if the credentials being used work to login to the cameras web interface.
Product
- Cloudvue Gateway
- Cloudvue Software v22.9.2
Steps to Reproduce
- From the Devices tab in Cloudvue Local (Settings > Devices)
- Scan For devices , select and add an Amcrest Camera
- When prompted enter username, password and add as ONVIF
Expected Results
- Camera adds
Actual Results
- Camera fails to add with an error message “Camera Save Failed … Invalid Username / Password”
Solution
- Create a user in the camera called “onvif” and use those credentials when adding the camera in Cloudvue Local.
Re: ONVIF authentication not working in newer cameras
Post by ckchessmaster ยป Wed Jan 18, 2023 12:58 pm