Installing 32-bit Enterprise System Manager (ESM) on 64-bit Ubuntu Linux System

To install ESM on a 64bit Ubuntu 12.04 Linux computer, complete the following steps:

Configuring a New System

  1. Set up a 64-bit Ubuntu 12.04 image.
  2. Install ia32-libs and postgresql.
  3. Use a remote database engine (or install Mysql/Postgresgl locally) to create a database.

Remote Setup

  1. Ensure that X Windows can be forwarded to anyone using Putty or SSH (install gedit).
  2. Use Filezilla to transfer the debian installer to the instance.
  3. Connect using Putty or SSH with X Windows forwarding enabled.

Installing ESM

  1. Install ESM with sudo dpkg -i exacqVisionEnterpriseSystemManager.deb (using the exact name of the file if different from what is shown here).
  2. Accept the defaults for port selection.
  3. Click YES on the warning message for 64-bit Architecture.
  4. Point ESM at the newly created database.
  5. Select No for migration and schema printing.
  6. Launch a browser and connect to ESM.
  7. Modify the admin account’s username and password.

<br>

Installing-32-bit-Enterprise-System-Manager-ESM-on-64-bit-Ubuntu-Linux-System.pdf