ExacqVision Enterprise

exacqVision Enterprise Manager features a web-based dashboard that provides at-a-glance status of the environment’s health and manage exacqVision servers deployed on the customer premise. Features include rules, alerts, software and licensing updates, config backups, camera inspection etc. Recordings are safeguarded with Enterprise Manager’s built-in failover solution that protects critical data. Enterprise Manager is available for free to work with exacqVision servers licensed at Enterprise level. This software is pre-installed on EM-Series servers or can be installed on third-party physical or virtual servers.