Description
Event Linking Time Triggers using custom days of the week are activating on the wrong day. They are triggering 1 day earlier so events set for Saturday are triggering on Friday and so on.
Tested Version
- exacqVision Server 22.12 – 22.03
Steps To Reproduce
- Create a new Event Linking action
- Set Event Type to Time Trigger
- Under Event Source select New
- Configure a time trigger
- Give the trigger a name
- Select a Start Time and End Time
- Set Frequency to Custom
- Select the current day of the week
- Set Action Target to Notify

Expected Results
- On the day and time specified in the Time Trigger
- Event Links Status switches from off to on
- An email is sent
Actual Results
- Event links status stays off
- An email is not received
Solution
- Downgrade to exacqVision Server version 22.09
NOTE: Fix will be available in exacqVision Server version 23.06
AES-425