Configuring the Time Server on Linux-based exacqVision Systems

To configure the time server on a Linux-based exacqVision system, complete the following steps:

  1. In exacqVision Client, make sure Enable Time Server is not selected on the Date/Time tab on the System Setup page.
  2. In a Terminal window, type sudo /etc/init.d/edvrserver stop to stop the exacqVision service.
  3. In a Terminal window, type sudo /etc/init.d/ntp start.
  4. Type sudo /etc/init.d/edvrserver start to start the exacqVision service.

On the System Setup page, Enable Time Server should now be selected and not greyed out.

Configuring-the-Time-Server-on-Linux-based-exacqVision-Systems.pdf