Profile Description: %1. Notification attempt return code= 26

Profile Descriptìon: %1. Notification attempt return code= 26

Description

%1 – This is the name of the Email Message Profile %BR% %BR%

Notifications are sent using curl, so the return codes are curl status/error codes. %BR%

Curl error 26 means “Read Error”

Notes

Notifications which include attaching a clip will attempt to create, then read a file locally on the Server. If there was a failure when the clip was created, you’ll see this error. Also, you could see this error due to a permissions limitation. %BR%
Other curl errors can be found here:%BR%
https://curl.se/libcurl/c/libcurl-errors.html