Profile Description: %1. Notification attempt return code= 7

Profile Descriptìon: %1. Notification attempt return code= 7

Description

%1 – This is the name of the Email Message Profile%BR% %BR%

Notifications are sent using curl, so the return codes are curl status/error codes. %BR%

Curl error 7 means “Couldn’t Connect”

Notes

Connection failures to SMTP servers result when the TCP connection to a given host/port fails. This could mean a firewall is blocking communication.%BR%
Other curl errors can be found here: %BR%
https://curl.se/libcurl/c/libcurl-errors.html