Categories
Exclude from Global Search Knowledge Support Log Level Support Warning exacqVision Server Categories Products Logs NotifyPI

Profile Description: %1. Notification attempt return code= 28

Profile Descriptìon: %1. Notification attempt return code= 28

Description

%1 – This is the name of the Email Message Profile %BR% %BR%

Notifications are sent using curl, so the return codes are curl status/error codes. %BR%

Curl error 28 means “Operation Timeout”

Notes

Timeouts to SMTP servers can result due to routing problems between the exacqVision Server and the SMTP Server, or a configuration problem, such as using the wrong address/port.