Geovision – Onvif Not Triggering Motion

Description

exacqVision Server is not detecting motion from Geovision cameras using the onvif plugin.  IP camera database indicates motion is supported  for the GV-TBL8810

Product 

  • exacqVision Server 22.09
  • Onvif Plugin  (onvifnvcpi.json)
  • Geovision Cameras
    • GV-TBL8810

Steps to Reproduce 

  • Add Geovision camera to exacq server
  • Configure motion on exacq and or the camera
  • Trigger motion

Expected Results 

  • Motion is triggered

Actual Results 

  • Motion is not triggered in exacqVision

Solution

WARNING – This is temporary and will not survive an upgrade of exacqVision Server Software

Before Changes
After Changes

Note:  See AES-216 for additional information