KT-1 Controller Firmware Must be v3.06.09 or Higher for Cloudvue Mode

Description

In addition to requiring a network with internet access the Kantech KT-1 controller must be running firmware v3.06.09 or higher to run in Cloudvue Mode.

Solution

To determine the current firmware version, access the KT-1 controller from a web browser.


Type https:// and the IPv4 address of the KT-1 or if using the MAC address type https://kt-xx-xx-xx where xx-xx-xx is the last six characters of the KT-1 controllers MAC address


Note: The MAC address can be found on a label located on the front of the KT-1 controller’s main board.

IMPORTANT

If the KT-1 is running a firmware lower than v2.09.02 you must first update to v2.09.02 before updating to v3.06.09 or higher. Firmware version 2.09.02 can be downloaded Here.


See the KT-1 Cloud User Guide for additional detailed instructions including how to update the KT-1 controllers firmware.