Exacq Mobile 3 app does not allow cameras to show Time stamps OSD of the server time while in a different TIME ZONE than the recorder

Description 

The Exacq Mobile 3 application does not show the OSD of cameras while the device is in a different time zone.

Product 

Exacq Mobile 3 application for both iPhone and Android.

Expected Results 

We should be able to account for when the Device is in a different time zone than the recorder while using the Exacq Mobile 3 application to reflect the camera times, in case searching video is required.

Actual Results 

The Exacq Mobile 3 application will show the cameras OSD timestamps as the time of the recorder.

Solution

If the need to search the time of an event is needed on the Exacq Mobile 3 application please keep in mind the difference between time zones.

At this time there is no solution.


AES-96
<br>