Re-installing an exacqVision Capture Card Driver

Important

  • Beginning 12/14/2021 extension of the SSA “Software Subscription Agreement” will be restricted on systems which have an eDVR capture board. In addition, starting with exacqVision Server version 22.06 the XDVPI plugin has been removed and systems where the plugin is present will be blocked from upgrading. In order to either extend the SSA or update to 22.06 or higher the board and the XDVPI plugin must be removed.
  • Beginning 06/14/2021 extension of the SSA “Software Subscription Agreement” will be restricted on systems using the Dahua DHVECxxxx capture board. The board must be removed in order to extend the SSA.

Note: If your exacqVision Utilities DVD is labeled with a software version 5.6.1.43456 or later, use the following procedure. If your DVD is labeled with an earlier version, skip ahead to the second procedure.


Instructions for exacqVision utilities DVD Versions 5.6.1.43456 and later

Linux

  1. Insert the exacqVision Utilities DVD into the optical drive of the server. The disc will auto-launch.
  2. Double-click BoardPrep.
  3. Type the admin password (admin256 is default).
  4. Press 1 to install the driver.
  5. Press Enter to exit.
  6. Open a Terminal window.
  7. To confirm the module loaded, type the command appropriate for your system:

    eDVR
    : lsmod | grep xdviomod
    sdvr, s7dvr, xsdvr
    : lsmod | grep s6stretch
    Dahua
    : lsmod | grep dm64xc
    tDVR: lsmod| grep Exacq

<br>

Windows

  1. Insert the exacqVision Utilities DVD into the optical drive of the server. The disc will auto-launch.
  2. Navigate to the Recovery folder and then the Maintenance folder.
  3. Right-click BoardPrep and select Run as Administrator.
  4. Select OK to run.
  5. Press Y to install the driver.
  6. Restart the server.
  7. To confirm the driver has been installed, open Device Manager and verify that the board appears without any yellow exclamation mark.

Instructions for exacqVision utilities DVD Versions earlier than 5.6.1.43456

Determine which capture card is installed

Linux

  1. Enter the following in Terminal: lspci|grep 18a2
  2. The output might look similar to this:

    05:00.0 Multimedia controller: Device 18a2:0026 (rev 01)

    The portion after “Device” identifies the capture card. Write down this device code and proceed to Step B.
  3. If you see no results, enter the following in Terminal: lspci|grep TriMedia
  4. The output might appear similar to this:

    Multimedia controller: Philips Semiconductors TriMedia TM-1300 (rev83)

    This is an eDVR card. Write down this information and proceed to Step B.
  5. If you still see no results and you are sure this is a hybrid system, please contact technical support.

<br>

Windows

  1. Open Device Manager. If the capture card driver is not installed, the card appears in the device list as Multimedia Controller under Other Devices.
  2. Right-click the Multimedia Controller entry and select Properties.
  3. On the Details tab, select Hardware IDs from the Property drop-down list.
  4. If the device is an exacqVision capture card, the returned Value should appear similar to the following:

    PCI\VEN_18A2&DEV_0026&SUBSYS_000018A2&REV_01

    The device code for the card in the example above is 18a2:0026, based on the numbers and letters immediate after VEN_ and DEV_. Write down your specific device code and proceed to Step B.
  5. If the card is an eDVR card, the returned Value should appear similar to this:

    PCI\VEN_1131&DEV_5402&CC_0480

    This is an eDVR card. Write down this information and proceed to Step B.
  6. If you do not see a Value similar to the ones listed above, and you are sure this is a hybrid system, try to find another Multimedia Controller in Device Manager or contact technical support.

<br>

Download the driver

  1. If you have Internet access, you can find the driver in the following location:

    https://exacq.com/support/downloads.html


    Otherwise, you can find the driver on the exacqVision Recovery CD that shipped with your system.
  2. Use the following table to determine which driver to download:
Device Code
(from Step A)
Card TypeInstaller TypeLinux FilenameWindows Filename
19e5:xxxxDHVRC8008HBDahuadahua.debN/A
19e5:3520DHVEC8016HB (see note 1)Dahuadahua.debN/A
TriMedia TM-1300N/A (see note 2)eDVRxdvapi.debxdvapi.exe
18a2:0002VRC6016SDVRsdvr.debsdvr.exe
18a2:000aVRC6016CSDVRsdvr.debsdvr.exe
18a2:002bVRC6016CSDVRsdvr.debsdvr.exe
18a2:0020VRC7016LSDVRs7dvr.debs7dvr.exe
18a2:0023VRC7008LSDVRs7dvr.debs7dvr.exe
18a2:0025VRC7032SDVRs7dvr.debs7dvr.exe
18a2:0026VRC7016LXSDVRs7dvr.debs7dvr.exe
18a2:002A7008ESDVRs7eDVR.debs7eDVR.exe
18a2:002B7016XESDVRs7eDVR.debs7eDVR.exe
18a2:1974xsDVR6516SDVRxsdvr.debxsdvr.exe
18a2:19e8xsDVR6632SDVRxsdvr.debxsdvr.exe
5851:8008TDVR8008tDVRtdvr.debtdvr-Setup.exe
5851:8016TDVR8016tDVRtdvr.debtdvr-Setup.exe
5851:8032TDVR8032tDVRtdvr.debtdvr-Setup.exe
Note 1: Beginning 06/14/2021 extension of the SSA “Software Subscription Agreement” will be restricted on systems using the Dahua DHVECxxxx capture board. The board must be removed in order to extend the SSA..

Note 2: Beginning 12/14/2021 extension of the SSA “Software Subscription Agreement” will be restricted on systems which have an eDVR capture board. In addition, starting with exacqVision Server version 22.06 the XDVPI plugin has been removed and systems where the plugin is present will be blocked from upgrading. In order to either extend the SSA or update to 22.06 or higher the board and the XDVPI plugin must be removed.

<br>

Install the driver

Linux

  1. Double click on the appropriate driver file found in Step B.
  2. Click Install Package.
  3. If asked for a password, enter admin256.
  4. After the installation is complete, click Close.
  5. Exit the package installer application by clicking the X in the upper-right corner of the window.

<br>

Windows

  1. Run the EXE file found in Step B.
  2. Open Device Manager.
  3. Verify that the board appears as a device without any yellow exclamation marks.

<br>

Note: For eDVR systems, you must run Control Center in Windows, or /usr/local/xdvapi/bin/xdvccl in Linux, to populate the device info in XDVAPI.ini.

<br>

Re-installing-an-exacqVision-Capture-Card-Driver.pdf