Categories
exacqVision Webservice Categories Products

Can ExacqVision Server run on Linux?

Yes, ExacqVision Server has been tested on the following:

  • Ubuntu 22.04 (64-bit)
  • Ubuntu 20.04 (64-bit)
  • Ubuntu 18.04 (64-bit)
  • Ubuntu 16.04 (64-bit)
  • Ubuntu 14.04 (64-bit or 32-bit with PAE1)
  • Ubuntu 12.04 (32-bit with PAE1)2
  • Ubuntu 10.04 (32-bit with PAE1)2

Version numbers are listed as YY.MM.

ExacqVision supports Ubuntu LTS releases only. Canonical provides LTS releases every two years. Long Term Support (LTS) lasts for a period of 10 years after release. ExacqVision will provide support for future LTS releases of Ubuntu as they become available.<br>

  1. PAE stands for Physical Address Extension, which allows 32-bit systems to use more than 4GB of memory.
  2. These versions are no longer receiving security updates from Canonical. At the end of long term support, future Exacq software releases will not be tested on these versions.

<br>