tDVR %1 video|audio %2 drop %3

tDVR %1 video|audio %2 drop %3

Description

%1 = The number of capture card in the system starting with 0. %BR% %2 = The analog input channel starting with 0. %BR%%3 = The amount of frames dropped. %BR% This log tells how many frames of audio or video were dropped and which board channel it occurred on.

Notes

If only 1 frame was dropped, it is likely due to poor quality video.If a group of frames is dropped. The frame buffer is filling up; check for resource limitations or anti-virus.