*** WSAEADDRINUSE – 10048 ***

*** WSAEADDRINUSE – 10048 ***

Description

Address already in use.

Notes

Typically, only one usage of each socket address (protocol/IP address/port) is permitted. This error occurs if an application attempts to bind a socket to an IP address/port that has already been used for an existing socket, or a socket that was not closed properly, or one that is still in the process of closing.