Profile description: %1 , Result: * DD HH:MM:SS %2 sendEmail.exe[*]: Email was sent successfully!
Description
%1 = Notification Profile name. %BR% %2 = System name. %BR% The Notification Profile triggered and successfully sent an email.
Notes
Not a problem, unless this occurs way too often. If so, check the Event Linking “Event Type” which triggers this profile. If it’s Video Motion, this will fire off every motion frame or event. Consider another Event Type, or set your Send Rate Limit to something other than 0 seconds on the Email Message Profile.