Categories
Knowledge Support Exclude from Global Search Log Level Support Warning exacqVision Server Categories Products Logs StreamPI

Client %1:%2 disconnected on receive (WSAECONNABORTED).

Client %1:%2 disconnected on receive (WSAECONNABORTED).

Description

%1 = Client machine IP address. %BR% %2 = Port number Client used to connect. %BR% This Windows Socket Error indicates that the Server-Client connection was aborted.

Notes

This indicates that the network connection between the Server and Client was aborted. This can be due to a congested network, or Anti-Virus interference either at the Client, or Server side. If the IP address is 127.0.0.1, it’s almost always Anti-Virus on the Server.