Client %1:%2 (Port) disconnected on receive (WSAECONNRESET).
Description
%1 = Client machine IP address. %BR% %2 = Port number Client used to connect. %BR% This Windows Socket Error indicates that the Server-Client connection was forcibly closed by the remote host.
Notes
This indicates that the network connection between the Server and Client was cut off unexpectedly. This can be due to a congested network, unexpected shutdown, or Anti-Virus interference either at the Client, or Server side. If the IP address is 127.0.0.1, it’s almost always Anti-Virus on the Server.