*** Current Video codec format for Input %1, Stream %2 is not supported. Please set the device to MJPEG, MPEG4 or H.264

*** Current Video codec format for Input %1, Stream %2 is not supported. Please set the device to MJPEG, MPEG4 or H.264

Description


%1 = Name of the camera %BR%

%2 = In the case of multi lens cameras, this is the stream ID %BR%
The camera is currently streaming in a codec that is not supported by exacqVision.

Notes

Change the stream codec to one supported or factory default the camera.