Categories
Exclude from Global Search Knowledge Support Log Level Warning Support exacqVision Server Categories Products Logs PsfPI

System %1 could not get record volume

System *** could not get record volume

Description

%1 = the stream id. %BR%
For that particular stream, we could not find a place to record it.

Notes

We try to have 1 GB of free space free to record to when we open a file. This is the warning we print if we can’t find that. It can happen at start up while the file plugin scans the drives to determine which files to delete. If it happens every 5 minutes, the drive doesn’t have enough free space to record 1GB * the number of devices in the system even after deleting all .ps and .psi files. %BR%
Very old versions of Server (pre 8.0) could result in this scenario.