PlugIn detected disk /c0/%1 has been removed

PlugIn detected disk /c0/%1 has been removed

Description

%1 = The port number of the disk. %BR%
A user may see this message under following circumstances – %BR% __1. A disk is removed from the system or %BR% __2. If a disk was saved to the config file but when the plugin was restarted, one of the saved disk was not found after rescanning the system. %BR% %BR% On some 3ware 9750 Linux systems, we have noticed that when a disk is replaced, the raid controller may change the disk name. This could result in #2 above, because the new disk has a new name.